REC.TRIG
Description
REC.TRIG starts the trigger according to the trigger type defined by REC.TRIGTYPE.
REC.TRIG sets the value of REC.DONE to 0.
After calling REC.TRIG, the data that was recorded by previous recording is deleted and cannot be retrieved.
No REC parameters can be set after a call to REC.TRIG until the recorder has finished or until REC.OFF is executed.
Examples
Code
If a trigger is set up, this command will arm the trigger. If the recording is "Immediate", this command will start the recording.
-->REC.TRIG
Context
For more information see Scope.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Command |
|
Units |
N/A |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
N/A |
|
See Also |
REC.RETRIEVE, REC.OFF |
|
Stored in Non Volatile Memory |
No |
Variants Supported
All variants are supported
|
Copyright © 2018 Kollmorgen |
|